:MEASure:JITTer:DEFine:RJSTabilize
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter
Command Syntax
:MEASure:JITTer:DEFine:RJSTabilize{? {ON | OFF | 1 | 0}
Query Response
{1 | 0}
Description
Selects RJ stabilization, which locks (stabilizes) the value of the measured RJ that is used in jitter measurements. Use RJ stabilization to prevent any uncorrelated non-Gaussian, non-periodic jitter from falsely contributing to any measured RJ value. Use the :MEASure:JITTer:DEFine:RJSValue command to enter the stabilization value in seconds. Use the :MEASure:JITTer:DEFine:RJSValue:GMRJ command to automatically enter the current measured RJ value. This RJ value will be locked in subsequent jitter measurements.