:MEASure:JITTer:DEFine:RJCValue

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter

Command Syntax

:MEASure:JITTer:DEFine:RJCValue  <value>

<value> is a double.

Query Syntax

:MEASure:JITTer:DEFine:RJCValue?

Description

Enters an RJ compensation value. Use the :MEASure:JITTer:DEFine:RJComp command to turn RJ compensation on.

The default setting is 0s, the minimum setting is 0s, and the maximum setting is 1s.

Common Numerical Child Commands

This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.