:MEASure:JITTer:DEFine:RJSValue

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter

Command Syntax

:MEASure:JITTer:DEFine:RJSValue  <value>

<value> is a double.

Query Syntax

:MEASure:JITTer:DEFine:RJSValue?

Description

Enters an RJ stabilization value. Use the :MEASure:JITTer:DEFine:RJSTabliize command to turn RJ stabilization on. Manually entering the RJ value, requires a two-part measurement. First, remove any sources of uncorrelated non-Gaussian, non-periodic jitter (for example, cross talk or non-periodic electromagnetic interference). Then, set RJ stabilization off and measure the RJ. Then, turn RJ stabilization on and reapply the sources of uncorrelated non-Gaussian, non-periodic jitter. One use of RJ stabilization is to prevent cross talk, from an adjacent channel, appearing as jitter. Use the :MEASure:JITTer:DEFine:RJSValue:GMRJ command to automatically enter the current measured RJ value. This RJ value will be locked in subsequent jitter measurements.

The default setting is 0s, the minimum setting is 0s, and the maximum setting is 1s.

Common Numerical Child Commands

This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.