:MEASure:JITTer:DEFine:LWIDth:PERCent

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter

Command Syntax

:MEASure:JITTer:DEFine:LWIDth:PERCent <percent>

Where <percent> is a double.

Query Syntax

:MEASure:JITTer:DEFine:LWIDth:PERCent?

Description

When the :MEASure:JITTer:DEFine:LWIDth parent command is set to PERCent for a PAM4 waveform, this command sets the amplitude level width as a percent of UI. Amplitude level width is used to determine the size of the window that is used for calculating Eye Height, Vertical Eye Closure (VEC), Eye Linearity (CEI), and Minimum RMS location. The percentage can range from 1% to 25%. The default setting is 5.0%.

Requires FlexDCA revision A.05.60 and above.