:MEASure:JITTer:DEFine:LWIDth:WINDow:GSDPercent
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter
Command Syntax
:MEASure:JITTer:DEFine:LWIDth:WINDow:GSDPercent <percent>
Where <percent> is a double.
Query Syntax
:MEASure:JITTer:DEFine:LWIDth:WINDow:GSDPercent?
Description
On PAM4 waveforms when the amplitude level window's width is based on a percentage (:MEASure:JITTer:DEFine:LWIDth command) and the shape of the window is selected to be Guassian (:MEASure:JITTer:DEFine:LWIDth:WINDow command), use :MEASure:JITTer:DEFine:LWIDth:WINDow:GSDPercent to specify the standard deviation (percent of UI)
Requires FlexDCA revision A.06.90 and above.