:MEASure:JITTer:DEFine:THReshold:PROBability

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter

Command Syntax

:MEASure:JITTer:DEFine:THReshold:PROBability <double>

Where <double> is the probability.

Query Syntax

:MEASure:JITTer:DEFine:THReshold:PROBability?

Description

When the jitter sampling-level setting is set to eye center (:MEASure:JITTer:DEFine:LEVel:TYPe), this command sets the probability value at which to determine the eye center on PAM4 signals. The default value is 1.0E-5. The minimum value is 1.0E-9. The maximum value is 10.0E-3.

Requires FlexDCA revision A.05.60 and above.