:MEASure:JITTer:DEFine:LWIDth:WINDow
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter
Command Syntax
:MEASure:JITTer:DEFine:LWIDth:WINDow {BOXCar | GAUSsian}
Query Syntax
:MEASure:JITTer:DEFine:LWIDth:WINDow?
Description
On PAM4 waveforms when the amplitude level window's width is based on a percentage (:MEASure:JITTer:DEFine:LWIDth command), use :MEASure:JITTer:DEFine:LWIDth:WINDow to specify the window shape: Boxcar or Gaussian.
If you specify a Gaussian window, use the :MEASure:JITTer:DEFine:LWIDth:WINDow:GSDPercent command to specify the standard deviation (percent of UI).
The query form of the command returns the current setting.
Requires FlexDCA revision A.06.90 and above.