:MEASure:JITTer:DEFine:THReshold:ESTiming
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter
Command Syntax
:MEASure:JITTer:DEFine:THReshold:ESTiming {CEYE | PELevel}
Query Syntax
:MEASure:JITTer:DEFine:THReshold:ESTiming?
Description
When the jitter sampling-level setting is set to eye center (:MEASure:JITTer:DEFine:LEVel:TYPe), sets the receiver sample timing to Independent Per Eye (PELevel) or Based on Center Eye (CEYE) for PAM4 waveforms. The default setting is CEYE.
Requires FlexDCA revision A.05.60 and above.