:MEASure:JITTer:DEFine:LWIDth
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter
Command Syntax
:MEASure:JITTer:DEFine:LWIDth {MINimum | PERCent}
Query Syntax
:MEASure:JITTer:DEFine:LWIDth?
Description
On PAM4 waveforms sets the amplitude level width that determines the size of the window that is used for calculating Eye Height, Vertical Eye Closure (VEC), Eye Linearity (CEI), and Minimum RMS location. The amplitude level width can be specified as a percentage of a UI (Unit Interval) or as the minimum resolution width window. This is corresponds to the Amplitude Level Width setting in the Jitter Mode Measurement Setup dialog.
MINimum- Specifies a minimum width window that is automatically be calculated.
PERCent(default setting)- Specifies the window's width based on a percentage of UI. Use the
:MEASure:JITTer:DEFine:LWIDth:PERCentcommand to enter the desired percentage in terms of UI. Use the:MEASure:JITTer:DEFine:LWIDth:WINDowcommand to select the shape of the window: Boxcar or Guassian. If Gaussian is selected, specify the standard deviation (percent of UI) using the:MEASure:JITTer:DEFine:LWIDth:WINDow:GSDPercentcommand.
The query form of the command returns the current setting.
Requires FlexDCA revision A.05.60 and above.