:MEASure:JITTer:DEFine:SIGNal
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter
Command Syntax
:MEASure:JITTer:DEFine:SIGNal{| {CLOCk | DATA}
Query Syntax
:MEASure:JITTer:DEFine:SIGNal{?
Description
Specifies the type of input signal: data (DATA) or clock (CLOCk). Use this command if a poorly-defined signal can not be automatically detected using :MEASure:JITTer:DEFine:SIGNal.
Example Command Sequence
:MEASure:JITTer:DEFine:SIGNal:AUTodetect OFF :MEASure:JITTer:DEFine:SIGNal CLOCk