:MEASure:JITTer:DEFine:TJBer

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter

Command Syntax

:MEASure:JITTer:DEFine:TJBer  <BER>

<BER> is a double.

Query Syntax

:MEASure:JITTer:DEFine:TJBer?

Description

Specifies the symbol-error-rate level for calculating Total Jitter (TJ) and Total Interference (TI). You can enter values from 1E-1 to 1E-18. The default value is 1E-12. If you enter 2.5E-3, the TJ measurement in the results table is labeled J2. If you enter 2.5E-10, TJ measurement in the results table is labeled J9.

Common Numerical Child Commands

This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.