:TDR:CALibration:AVERages
Instrument:
DCA-X
Meas. mode:
TDR
Package License:
L-SNT
Flex Apps:
FlexDCA
Command Syntax
:TDR:CALibration:AVERages <count>
<count> is an int.
Query Syntax
:TDR:CALibration:AVERages?
Description
Sets the number of waveforms averaged during TDR calibrations. The default number of averages is 128.
Requires FlexDCA revision A.04.00 and above.