:TDR:CALibration:STEP:SELect
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:CALibration:STEP:SELect <step>
<step> is an int.
Description
This command allows you to select a calibration step, during a TDR calibration. Normally, steps progress from the lowest to the highset number. However, you can use this command to perform the steps in a different order or to skip a step as shown in the following picture. This pictures shows that step 3 was performed after step 1 and that step 2 is selected as the next step.
Requires FlexDCA revision A.04.00 and above.