:TDR:CALibration:DUT:NOCSteps?
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Query Syntax
:TDR:CALibration:DUTN:NOCSteps?
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Description
Queries the number of calibrations steps required for the currently configured calibration. The number of steps is affected by the following items:
- Calibration method used (
:TDR:CALibration:DUT:METHod). There can be a significant reduction of the required steps when an ECal-Based calibration is used rather than a mechanical-based SOLT or SLT calibration. - Number of time-domain responses selected.
Requires FlexDCA revision A.04.00 and above.