:TDR:CALibration:DUT:SENDed:PORT{1:16}:CONNector
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:CALibration:DUTN:SENDed:PORT{1:16}:CONNector {M350 | F350 | M292 | F292 | M240 | F240 | M185 | F185 | PROBe}
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Query Syntax
:TDR:CALibration:DUTN:SENDed:PORT{1:16}:CONNector?
Description
Enters the RF connector type for each of the DUT's ports. Supported connector types include 1.85 mm, 2.4 mm, 2.92 mm, and 3.5 mm (both male and female). To indicate if the connector types on all of the DUT's ports match or not, use the :TDR:DUT:ACMatch command.
| Connector Type | Command Argument | |
|---|---|---|
| Male | Female | |
| 3.5 mm | M350 | F350 |
| 2.92 mm | M292 | F292 |
| 2.4 mm | M240 | F240 |
| 1.85 mm | M185 | F185 |
| Probe | PROBe | |
Requires FlexDCA revision A.04.00 and above.