:TDR:CALibration:SDONe
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:CALibration:SDONe
Description
During the TDR/TDT Calibration wizard, sets an interupt to indicate that the next wizard step is viewed. Start the calibration using the :TDR:CALibration:DUT:STARt command.
Requires FlexDCA revision A.04.00 and above.