:TDR:CALibration:UCURrent
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:CALibration:UCURrent
Description
When performing a TDR calibration using mechanical standards (SOLT or SLT), a step may be interpreted as having been improperly performed. For example, you may have connected an open when the step specified a short as shown in the following picture. You can either repeat the step or use the :UCURrent command to indicate that the calibration should use the current results for the step. This is equivalent to clicking Use Current in the TDR/TDT Calibration dialog.
Requires FlexDCA revision A.04.00 and above.