:TDR:CALibration:DUT:SENDed:PORT:CKIT

Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter

Command Syntax

:TDR:CALibration:DUTN:SENDed:PORT{1:16}:CKIT <string>

Where N indicates one of 16 possible DUT setups. For example, :DUT4.

The following <string> arguments (calibration kits) are supported. The string argument is not case sensitive.

  • 85052B/D 3.5 mm
  • 85056A/D 2.4 mm
  • 85058B/E 1.85 mm
  • 85052K E01/E02 (2.92 mm Broadband Load)
  • Maury 8770D (2.92 mm Broadband Load)
  • Maury 8770C (2.92 mm Sliding Load)
  • Generic 2.92 (2.92 mm calibration kit)
  • Generic 3.5 (3.5 mm calibration kit)
  • Generic 2.4 (2.4 mm calibration kit)
  • Generic 1.85 (1.85 mm calibration kit)
  • Generic Probe (Probe Calibration kit)

Query Syntax

:TDR:CALibration:DUTN:SENDed:PORT{1:16}:CKIT?

Description

Enters the calibration kit that is to be used during a TDR calibration for each of the DUT's ports. The :PORT{1:16} portion of the command string identifies a specific DUT port. For single-ended DUTs, :PORT1 identifies port 1, :PORT2 identifies port 2, :PORT3 identifies port 3, and so on. For differential DUTs, selecting the correct port number in the command is slightly more complicated. The port numbers are identified in numerical order starting with the positive sides of the first input port and its associated output port. Then, the negative sides of the same ports are identified This continues with the next input and outputs ports. The following table shows the port numbering for a six-port DUT.

Port ID Numbers for 6-Port Differential DUT
:PORT
Command
DUT Port DUT DUT Port :PORT
Command
:PORT1 1+ 2+ :PORT2
:PORT3 1– 2– :PORT4
:PORT5 3+ 4+ :PORT6
:PORT7 3– 4– :PORT8
:PORT9 5+ 6+ :PORT10
:PORT11 5– 6– :PORT12

The supported kits and their associated string arguments are listed in the following table. To indicate if the calibration kit to be used for each of the DUT's ports is the same or not, use the :TDR:CALibration:DUT:SKAPorts command.

Supported Calibration Kits for Each Type of Port Connector
Calibration Kits Port Connector
3.5 mm 2.92 mm 2.4 mm 1.85 mm Probe
85052B/D 3.5 mm ♦ ♦
85056A/D 2.4 mm ♦ ♦
85058B/E 1.85 mm ♦ ♦
Maury 8770C (2.92 mm Sliding Load) ♦ ♦
Maury 8770D (2.92 mm Broadband Load) ♦ ♦
Generic 2.92 (2.92 mm calibration kit) ♦ ♦
Generic 3.5 (3.5 mm calibration kit) ♦ ♦
Generic 2.4 (2.4 mm calibration kit) ♦ ♦
Generic 1.85 (1.85 mm calibration kit) ♦ ♦
Generic Probe (Probe Calibration kit) ♦

Requires FlexDCA revision A.04.00 and above.