:TDR:CALibration:ATIMebase
Instrument:
DCA-X
Meas. mode:
TDR
Package License:
L-SNT
Flex Apps:
FlexDCA
Command Syntax
:TDR:CALibration:ATIMebase {ON | OFF}
Query Syntax
:TDR:CALibration:ATIMebase?
Description
Configures a TDR calibration so that the fixture length is automatically determined. This is the default setting. If you turn this setting off, use the following three commands to manually set the time window:
- :TIMebase:SCALe
- Sets the seconds-per-division on the display's x-axis.
- :TIMebase:POSition
- Sets the time value in seconds at the timebase reference which, by default, is two divisions from the left side of the display.
- :TIMebase:REFerence
- By default, the TDR time reference is set to the second division from the left edge of the display. Changing the reference to the center of the display is not recommended. The horizontal reference point defines a specific delay value relative to the trigger event.
Requires FlexDCA revision A.04.00 and above.