:TDR:CALibration:DUT:CLEar
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:CALibration:DUTN:CLEar
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Description
Clears and TDR calibration data that have been imported from a TDR calibration file (*.tdrx). TDR calibration data is imported using the :TDR:CALibration:DUT:CDFName command.
Requires FlexDCA revision A.04.00 and above.