:TDR:CALibration:DUT:FDRSet
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:CALibration:DUTN:FDRSet
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Description
Selects all available time-domain parameter responses for a TDR calibration. Use the :DRSet sibling command to select specific time-domain parameters and the :CDRSet sibling command to clear all currently selected time-domain parameters.
Requires FlexDCA revision A.04.00 and above.