:TDR:CALibration:DUT:ENABle
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:CALibration:DUTN:ENABle {ON | OFF}
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Query Syntax
:TDR:CALibration:DUTN:ENABle?
Description
When a valid TDR calibration file is imported using the TDR:CALibration:DUT:CDFName command, use this command to enable and disable the use of the imported calibration. This is equivalent to the Enable button on the TDR Setup dialog that is displayed after a calibration file is imported.
Requires FlexDCA revision A.04.00 and above.