:TDR:CALibration:DUT:LOAD:FNAMe
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:CALibration:DUTN:LOAD:FNAMe "<path substitution string>\subfolder\filename"
Where:
- N indicates one of 16 possible DUT setups. For example,
:DUT4. - "<path substitution string> is a string that expands into a specific file path. For example, %USER_DATA_DIR%.
- "subfolder" is an optional path folder. For example, %USER_DATA_DIR%\TDR Calibration.
- "filename" is a string without the filename extension.
Query Syntax
:TDR:CALibration:DUTN:LOAD:FNAMe?
Description
Stores the name of the TDR calibration file (.tdrx) that will be imported by the :TDR:CALibration:LOAD parent command. To clear the filename, send this command with an empty string.
Requires FlexDCA revision A.04.00 and above.
Example Command Sequence
:TDR:CALibration:DUT:LOAD:FNAMe "%USER_DATA_DIR%\TDR Calibration\SE 4Port_2014-10-23_1" :TDR:CALibration:DUT:LOAD