:TDR:CALibration:DUT:CRSet
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Query Syntax
:TDR:CALibration:DUTN:CRSet?
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Description
Returns a list of available time-domain parameters to include in a TDR calibration. The list is a comma separated list of time-domain parameters with an underscore (_) character between the numbers. For example, the argument for an T21 parameter is T2_1. Use the :DRSet sibling command to select specific time-domain parameters. To select all available time-domain parameter responses, use the :FDRSet sibling command. To clear all selected time-domain parameters, use the :CDRSet sibling command.
Requires FlexDCA revision A.04.00 and above.