:TDR:CALibration:DUT:CDATa:REASon
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Query Syntax
:TDR:CALibration:DUTN:CDATa:REASon?
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Description
Returns a message about the current TDR calibration. For a correct calibration, the date that the calibration was created is returned. For example,
"Created: 10/23/2014 13:41:00"
For an invalid calibration, an informational message is returned such as these examples:
"Please select a file." "Incorrect module configuration."
Use the parent :TDR:CALibration:DUT:CDATa command, to return the state of the calibration.
Requires FlexDCA revision A.04.00 and above.