:TDR:CALibration:DUT:RDUT
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:CALibration:DUTN:RDUT
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Description
Changing a DUT-based TDR Setup after a valid TDR calibration is enabled, may result in calibration data that no longer matches the setup. In this situation, use this command to restore the TDR Setup so that it is once again compatible with the calibration.
Requires FlexDCA revision A.04.00 and above.