:TDR:CALibration:DUT:LOAD
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:CALibration:DUTN:LOAD
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Description
Imports the TDR calibration data from the TDR calibration file named with the :FNAMe child command. Each time that a TDR calibration is performed for a particular DUT setup, a calibration file (*.tdrx) is saved in the \TDR Calibration folder. The files are saved for a specific TDR module, DUT setup, and calibration setup. To clear the filename, send this command with an empty string. To clear the imported calibration data from memory so that it will not be applied, use the :TDR:CALibration:DUT:CLEar command.
Requires FlexDCA revision A.04.00 and above.
Example Command Sequence
:TDR:CALibration:DUT:LOAD:FNAMe "D:\user files\TDR Calibration\SE 4Port_2014-10-23_1.tdrx" :TDR:CALibration:DUT:LOAD