:TDR:CALibration:DUT:SKAPorts
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:CALibration:DUTN:SKAPorts {ON | OFF}
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Query Syntax
:TDR:CALibration:DUTN:SKAPorts?
Description
Indicates if a single calibration kit is used when performing a TDR calibration. When ON is selected, all of the port connector definitions are set to the same type that has been entered for Port 1.
ON- A single calibration kit is used during the calibration.
OFF- Multiple calibration kits are used during the calibration. To specify the calibration kit used for each port, use the
:TDR:CALibration:DUT:SENDed:PORT:CKITcommand.
Requires FlexDCA revision A.04.00 and above.