:TDR:CALibration:STEP:COUNt?
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Query Syntax
:TDR:CALibration:STEP:COUNt?
Description
Queries the total number of steps for the currently configured calibration. Use the :TDR:CALibration:STEP? to return the number of the current step being executed in the TDR/TDT calibration. The number of steps for a calibration is affected by the following items:
- Calibration method used (
:TDR:CALibration:DUT:METHod) - Number of time-domain responses selected
Requires FlexDCA revision A.04.00 and above.