:TDR:CALibration:DUT:METHod
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:CALibration:DUTN:METHod {SOLT | SLT | ECAL}
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Query Syntax
:TDR:CALibration:DUTN:METHod?
Description
Select the method used to perform the TDR calibration. Selections are Short-Open-Load-Thru (SOLT), Short-Load-Thru (SLT), and ECal-Based (ECAL). The calibration is performed for the indicated DUT.
SOLTorSLT- When a
SOLTorSLTcalibration is selected, use the:TDR:CALibration:DUT:SENDed:PORT:CKITand:TDR:CALibration:DUT:SENDed:PORT:CKITcommands to specify the DUT connection types and calibration kit used. ECAL- When an ECal-Based calibration is selected, use the Configure ECal Adapter for DUT wizard to specify any adapters that are required to insert the ECal module into the test setup in place of the DUT. Use the
:TDR:ADAPters:STARtcommand to start the wizard. Use the:TDR:ADAPters:CHARcommand to select a characterization for the ECal module.
Requires FlexDCA revision A.04.00 and above.