:TDR:CALibration:DUT:CONFig:REASon
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Query Syntax
:TDR:CALibration:DUTN:CONFig:REASon?
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Query Response
<string>
Description
Returns a string that indicates the reason that a TDR calibration setup is invalid. This is the same information string that is shown at the top of the TDR Calibration Setup dialog, as shown in the following picture.
The following is an example of a returned string:
Port 2 connector is incompatible with the selected calibration kit.
Although a more detailed message can be read by clicking the Details button, there is no remote command for returning the detailed message. For the example message above, the more detailed message would be:
The calibration kit selected for Port 2 does not contain any standards that can mate to the selected connector type. Select a different calibration kit or correct the connector type specified for Port 2.
Requires FlexDCA revision A.04.00 and above.