:TDR:CALibration:DUT:STARt
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:CALibration:DUTN:STARt
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Description
In TDR mode, starts the TDR/TDT Calibration wizard for the specified DUT. Use the :TDR:CALibration:SDONe command to set an interupt that indicates when the next wizard step is viewed.
Requires FlexDCA revision A.04.00 and above.