:TDR:DUT:ACMatch
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:DUT{1:16}:ACMatch {ON | OFF}
Query Syntax
:TDR:DUT{1:16}:ACMatch?
Description
Indicates if the connector types on all of the DUT's ports match.
ON- All of the DUT's port use the same type of RF connector. When
ONis selected, all of the port connector definitions are set to the same type that has been entered for Port 1. OFF- At least on of the DUT's ports has an RF connector that is different from the rest of the ports. To specify the each of the DUT's connectors, use the
:TDR:CALibration:DUT{1:16}:SENDed:PORT{1:16}:CONNectorcommand.
Requires FlexDCA revision A.04.00 and above.