:EMODules:AWGenerator:AUPDate
AWG Instrument:
M8194/5/6A
M8199A/B
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
Licensed Feature:
F-AWG
Waveform type:
NRZ
PAM4/6/8
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:EMODules:AWGenerator{1:8}:AUPDate {ON | OFF | 1 | 0}
Where {1:8} identifies slot number which is associated with an AWG instrument.
Query Syntax
:EMODules:AWGenerator{1:8}:AUPDate?
Query Response
{ON | OFF }
Description
When on, FlexDCA automatically syncs FlexDCA's Arbitrary Waveform Generator (AWG) extended module's settings with the AXIe AWG module's settings. With automatic updating, you do not neet to manually "push" the settings to the AWG using the :EMODules:AWGenerator:SEND command or from FlexDCA's AWG Setup dialog, using the Send to Instrument button. The default setting is OFF.
Use an *OPC? query to pause program execution while waiting for this command to execute.
Requires FlexDCA revision A.06.00 and above. With revision A.07.50, the default state was changed from ON to OFF.
Example Command
:EMODules:AWGenerator3:AUPDate ON