:EMODules:AWGenerator:CLOCk:SMARker:OENable
AWG Instrument:
M8194/5/6A
M8199A/B
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
Licensed Feature:
F-AWG
Waveform type:
NRZ
PAM4/6/8
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:EMODules:AWGenerator{1:8}:CLOCk:SMARker:OENable {ON | OFF}
Where {1:8} identifies slot number which is associated with an AWG instrument.
Query Syntax
:EMODules:AWGenerator{1:8}:CLOCk:SMARker:OENable?
Query Response
{ON | OFF}
Description
For an M8199A/B Arbitrary Waveform Generator (AWG) extended module, enables (ON) or disables (OFF) the clock Sample Marker Out ports.
Requires FlexDCA revision A.07.60 and above.
Example Command
:EMODules:AWGenerator6:CLOCk:SMARker:OENable ON