:EMODules:AWGenerator:FORMat

AWG Instrument:
M8194/5/6A
M8199A/B
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
Licensed Feature:
F-AWG
Waveform type:
NRZ
PAM4/6/8
Flex Apps:
FlexDCA
FlexRT

Command Syntax

:EMODules:AWGenerator{1:8}:FORMat {NRZ | PAM4 | PAM6 | PAM8}

Where {1:8} identifies slot number {1:8} which is associated with an AWG extended module.

Query Syntax

:EMODules:AWGenerator{1:8}:FORMat?

Query Response

 {NRZ | PAM4 | PAM6 | PAM8}

Description

Selects the waveform format for an Arbitrary Waveform Generator (AWG) extended module's channel output: NRZ, PAM4, PAM6, or PAM8. This setting is applies to all AWG channel outputs.

Requires FlexDCA revision A.06.00 and above. Support for PAM6 and PAM8 was added in FlexDCA revision A.08.30.

Example Command

:EMODules:AWGenerator6:FORMat PAM4