:EMODules:AWGenerator:CLOCk:SMARker:RATio
AWG Instrument:
M8194/5/6A
M8199A/B
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
Licensed Feature:
F-AWG
Waveform type:
NRZ
PAM4/6/8
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:EMODules:AWGenerator{1:8}:CLOCk:SMARker:RATio {SUB4 | SUB8 | SUB16 | SUB32 | SUB64}
Where {1:8} identifies slot number which is associated with an AWG instrument.
Query Syntax
:EMODules:AWGenerator{1:8}:CLOCk:SMARker:RATio?
Query Response
{SUB4 | SUB8 | SUB16 | SUB32 | SUB64 | INValid}
Description
For an M8199A/B Arbitrary Waveform Generator (AWG), sets or returns the divide ratio between the AWG's clock on the Sample Marker Out port compared to the AWG's current sample rate. For example, if the sample rate is 200 GHz, and the sample marker ratio is set to SUB4 (1:4 subrate), then the Sample Marker Out port will generate a 50 GHz clock. To return the frequency of the clock at the Sample Marker Out port, use the :EMODules:AWGenerator:CLOCk:SMARker:FREQuency? query.
The command arguments and returned values are:
- SUB4
- The clock divide ratio is 1:4.
- SUB8
- The clock divide ratio is 1:8.
- SUB16
- The clock divide ratio is 1:16.
- SUB32
- The clock divide ratio is 1:32.
- SUB64
- The clock divide ratio is 1:64.
- INValid
- There is no AWG present, or the current AWG doesn't have a
Sample Marker Outport.
Requires FlexDCA revision A.07.60 and above.
Example Command Sequence
:EMODules:AWGenerator6:CLOCk:SMARker:RATio SUB8 clk_frequency = ':EMODules:AWGenerator6:CLOCk:SMARker:FREQuency?'