:EMODules:AWGenerator:FNAMe

AWG Instrument:
M8194/5/6A
M8199A/B
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
Licensed Feature:
F-AWG
Waveform type:
NRZ
PAM4/6/8
Flex Apps:
FlexDCA
FlexRT

Command Syntax

:EMODules:AWGenerator{1:8}:FNAMe "filename"

Where {1:8} identifies slot number which is associated with an AWG instrument.

Where "filename" is a string.

Query Syntax

:EMODules:AWGenerator{1:8}:FNAMe?

Query Response

"filename"

Description

Specifies the file name, path, and extension of a FlexDCA waveform file that you want to download to an Arbitrary Waveform Generator (AWG) extended module. To actually download the waveform file, use the :EMODules:AWGenerator:WTYPe command with the FILE argument. After downloading the file, use the :EMODules:AWGenerator:STATus query to confirm that the AWG accepted the file and successfully updated.

The default folder for storing waveform files is in %USER_DATA_DIR%\Waveforms as shown in this pictures. It is good practice to include a path substitution string with the filename. For example, %USER_DATA_DIR%\Waveforms\filename.

User-Data Folders

File names must include a path when using the child :FNAMe command. The :FNAMe command is not affected by a Default Setup or Factory Preset.

Specifying a path using a path substitution string in the filename ensures that the file will be saved in (or loaded from) the standard user-data folder. Failure to use a path substitution string may result either in a file created in an parent folder or a file error.

Requires FlexDCA revision A.06.00 and above.

Example Command

:EMODules:AWGenerator6:FNAMe "CH1_81141A_10.3125Gbps_PRBS7.csv"