:EMODules:OPTimization:AWGenerator:SDONe
AWG Instrument:
M8194/5/6A
M8199A/B
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
Licensed Feature:
F-AWG
Waveform type:
NRZ
PAM4/6/8
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:EMODules:OPTimization:AWGenerator:SDONe?
Description
During the AWG waveform optimization wizard, sets an interupt to indicate the next wizard step is viewed. Send this query after the :AWGenerator:OPTimization:STARt and :OPTimization:AWGenerator:CONTinue commands.
Requires FlexDCA revision A.06.40 and above.
Example Command
:EMODules:OPTimization:AWGenerator:SDONe?