:EMODules:AWGenerator:MODE

AWG Instrument:
M8194/5/6A
M8199A/B
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
Licensed Feature:
F-AWG
Waveform type:
NRZ
PAM4/6/8
Flex Apps:
FlexDCA
FlexRT

Command Syntax

:EMODules:AWGenerator{1:8}:MODE {BASic | ADVanced}

Where {1:8} identifies slot number {1:8} which is associated with an AWG extended module.

Query Syntax

:EMODules:AWGenerator{1:8}:MODE?

Query Response

 {BAS | ADV}

Description

Selects the configuration mode (Basic or Advanced) or the specified Arbitrary Waveform Generator (AWG). The following arguments are used:

BASic
In Basic mode, waveform symbol rate and pattern settings apply to all four AWG channels. Warnings are displayed if your settings do not result in valid AWG waveforms.
ADVanced
In Advanced mode, waveform symbol rate and pattern settings can be different for each AWG channel. In addition, the AWG Optimization Wizard automatically switches the AWG Setup to Advanced mode and applies the optimized waveforms to each Data channel.

Use an *OPC? query to pause program execution while waiting for this command to execute.

Requires FlexDCA revision A.06.40 and above.

Example Command Sequence

For the AWG in slot 5, the following sequence of commands places the AWG setup into Basic mode, runs the optimization wizard, and saves the optimized waveform in the "Waveforms\OptimizedWaveform_Setup2.csv" file. The AWG's channel 3 is associated with the DCA-X's input channel 1B.

:EMODules:AWGenerator5:MODE BASic;*OPC?  //  Place AWG setup dialog in Basic mode.
:EMODules:AWGenerator5:OPTimization:FILE3 "OptimizedWaveform_Setup2.csv"   //  File to create.
:EMODules:AWGenerator5:OPTimization:CHANnel3 CHAN1B  //  Associate AWG channel 3.
:EMODules:AWGenerator5:OPTimization:STARt;*OPC?  //  Run the optimization wizard