:EMODules:AWGenerator:CLOCk:SAMPle:FREQuency?
AWG Instrument:
M8194/5/6A
M8199A/B
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
Licensed Feature:
F-AWG
Waveform type:
NRZ
PAM4/6/8
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:EMODules:AWGenerator{1:8}:CLOCk:SAMPle:FREQuency?
Where {1:8} identifies slot number which is associated with an AWG instrument.
Query Response
<frequency>
Description
For an M8199A/B Arbitrary Waveform Generator (AWG) extended module, returns the frequency at the Sample Clk Out ports.
Requires FlexDCA revision A.07.60 and above.
Example Command
:EMODules:AWGenerator6:CLOCk:SAMPle:FREQuency?