Arbitrary Waveform Generator

AWG Instrument:
M8194/5/6A
M8199A/B
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
Licensed Feature:
F-AWG
Waveform type:
NRZ
PAM4/6/8
Flex Apps:
FlexDCA
FlexRT

AWG Commands

The AWG commands apply to M8194/5/6A and M8199A/B Arbitrary Waveform Generator (AWG) extended modules. To configure the AWG you'll use the commands in this subsystem and the some of the commands from the :SOURce subsystem as noted in this topic.

Establish FlexDCA-to-AWG SFP Connection Commands

Always send the :EMODules:SLOT:SELection command first to assign the AWG to a FlexDCA slot. If the AWG is not assigned to a slot, sending any other connection commands will result in an error.

Defining AWG Waveform Commands

The AWG waveforms can be generated from either a FlexDCA waveform file that is downloaded to the AWG or from waveform parameter settings.

If you select to define the AWG waveform by parameter settings, use the following commands which are equivalent to making selections in the AWG setup dialogs. Note that configuring the waveform is done by combination of commands located this subsystem and in the :SOURce subsystem:

Universal AWG Channel Output Commands

Individual AWG Channel Output Commands

The following commands are located in the :SOURce subsystem.

Optimize Waveforms Commands

Clock Commands

Synchronizing FlexDCA/AWG Settings Commands

By default, FlexDCA's setting are automatically kept in sync with the AXIe AWG module's settings:

Example Command Sequence for connecting AWG:

:EMODules:SLOT6:SELection AWGenerator
:EMODules:AWGenerator6:SADDress "lan,4880;hislip[WINDOWS-6ISM873]:hislip0"
:EMODules:SLOT6:ADDRess SICL
:EMODules:SLOT6:CONNect;*OPC?