:EMODules:AWGenerator:OPTimization:STATus

AWG Instrument:
M8194/5/6A
M8199A/B
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
Licensed Feature:
F-AWG
Waveform type:
NRZ
PAM4/6/8
Flex Apps:
FlexDCA
FlexRT

Query Syntax

:EMODules:OPTimization:AWGenerator{1:8}:STATus?

Where {1:8} identifies slot number which is associated with an AWG instrument.

Query Response

{CORR | INV}
CORR
The AWG is correctly setup for optimization.
INV
The optimization setup is invalid.

Description

Queries the status of the AWG optimization wizard. Use the :EMODules:AWGenerator:OPTimization:STATus:REASon? child query to determine the reason for an invalid or questionable connection.

Requires FlexDCA revision A.06.40 and above.

Child Commands