:EMODules:AWGenerator:CLOCk:SMARker:FREQuency?

AWG Instrument:
M8194/5/6A
M8199A/B
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
Licensed Feature:
F-AWG
Waveform type:
NRZ
PAM4/6/8
Flex Apps:
FlexDCA
FlexRT

Query Syntax

:EMODules:AWGenerator{1:8}:CLOCk:SMARker:FREQuency?

Where {1:8} identifies slot number which is associated with an AWG instrument.

Query Response

<frequency>

Description

For an M8199A/B Arbitrary Waveform Generator (AWG) extended module, returns the frequency at the sample marker for the Sample Marker Out ports. To return the clock pattern ratio of the signal at the Sample Marker Out ports, use the :EMODules:AWGenerator:CLOCk:SMARker:RATio? query.

Requires FlexDCA revision A.07.60 and above.

Example Command

:EMODules:AWGenerator6:CLOCk:SMARker:FREQuency?