:EMODules:AWGenerator:SEND

AWG Instrument:
M8194/5/6A
M8199A/B
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
Licensed Feature:
F-AWG
Waveform type:
NRZ
PAM4/6/8
Flex Apps:
FlexDCA
FlexRT

Command Syntax

:EMODules:AWGenerator{1:8}:SEND

Where {1:8} identifies slot number which is associated with an AWG instrument.

Description

If automatic AWG updating is turned off, pushes the current FlexDCA waveform settings to the AWG. This is the same action as pressing the Send to Instrument button from FlexDCA's AWG Setup dialog. To turn on and off automatic AWG updating, use the :EMODules:AWGenerator:AUPDate command. After sending the :EMODules:AWGenerator:SEND command, confirm that the AWG is correctly updating using the :EMODules:AWGenerator:STATus.

Use an *OPC? query to pause program execution while waiting for this command to execute.

Requires FlexDCA revision A.06.00 and above.

Example Command

:EMODules:AWGenerator6:SEND