:EMODules:OPTimization:AWGenerator:CANCel
AWG Instrument:
M8194/5/6A
M8199A/B
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
Licensed Feature:
F-AWG
Waveform type:
NRZ
PAM4/6/8
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:EMODules:OPTimization:AWGenerator:CANCel
Description
Cancels the AWG waveform optimization wizard. This command is equivalent to clicking the Cancel button in the wizard.
Requires FlexDCA revision A.06.40 and above.
Example Command
:EMODules:OPTimization:AWGenerator:CANCel