:EMODules:AWGenerator:OPTimization:ITERations
AWG Instrument:
M8194/5/6A
M8199A/B
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
Licensed Feature:
F-AWG
Waveform type:
NRZ
PAM4/6/8
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:EMODules:AWGenerator{1:8}:OPTimization:ITERations {1:8}
Where {1:8} identifies slot number {1:8} which is associated with an AWG extended module.
Where {1:8} argument specifies the number of iterations.
Description
For the AWG optimization wizard, sets the number of iterations used by the optimization wizard (:EMODules:AWGenerator:OPTimization:STARt). Up to eight iterations can be specified. The default value is 1. While electrical setups usually require only one iteration, optical setups may need several iterations. Set the number of iterations before running the optimization wizard.
Requires FlexDCA revision A.06.40 and above.
Example Command
:EMODules:AWGenerator6:OPTimization:ITERations 4