:EMODules:AWGenerator:STATus?
AWG Instrument:
M8194/5/6A
M8199A/B
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
Licensed Feature:
F-AWG
Waveform type:
NRZ
PAM4/6/8
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:EMODules:AWGenerator{1:8}:STATus?
Where {1:8} identifies the slot number which is associated with an AWG instrument.
Query Response
{CORR | INV | QUES}
- CORR
- The settings in the AWG's memory are correct and matches the setting shown in the AWG Setup dialog.
- INV
- The settings in the AWG Setup dialog are invalid and cannot be sent to the AWG's memory.
- QUES
- The settings in the AWG setup dialog have not been pushed to the AWG extended module. This can happen if the dialog's Auto Update setting is not selected (
:EMODules:AWGenerator:AUPDate).
Description
Queries the status of the connection to an Arbitrary Waveform Generator (AWG) extended module. Use the :EMODules:AWGenerator:STATus:REASon? child query to determine the reason for an invalid or questionable connection. The AWG can become invalid in the following conditions:
- A corrupt or incompatible waveform file has been downloaded to the AWG. For example, the file's symbol rate is too high.
- The LAN connection to the AWG has failed.
Requires FlexDCA revision A.05.60 and above.
Example Command
:EMODules:AWGenerator6:STATus?