:TDR:ASNaming
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:ASNaming {ON | OFF}
Query Syntax
:TDR:ASNaming?
Description
Turns automatic signal naming on Waveform content windows on or off. This determines if waveforms are identified in the displayed window legend by channel (OFF) or by the DUT's port name (ON). The default setting is on. This setting does not affect the legend on other TDR Mode content windows. When signal naming is turned on, the default labels (for example, "Port") are displayed unless you have changed them using the :TDR:DUT:SENDed:PORT:UNAMe command. On differential signals, use the :TDR:DUT:ADPNaming command to specify custom port naming by individual (+/–) ports or differential ports.
| Stimulus Mode | ASNaming OFF | ASNaming ON | ||
|---|---|---|---|---|
| Default Connector Labels |
Custom Connector Labels |
|||
| Single-Ended |
|
|
|
|
| Differential |
|
|
ADPNaming OFF (Custom Diff +/– Labels) |
ADPNaming ON (Custom Diff Port Labels) |
|
|
|||
Requires FlexDCA revision A.04.00 and above.
Example Command
:TDR:ASNaming ON