:TDR:DUT:ACONnect
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:DUT{1:16}:ACONnect
Where {1:16} indicates one of 16 possible DUT setups.
Description
When setting up a DUT for TDR measurements, automatically connects available TDR channels to ports on the DUT. To manually connect the channels to the DUT's ports, use the :TDR:CHANnel:DUT and :TDR:CHANnel:PORT commands.
Requires FlexDCA revision A.04.00 and above.